{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many custom html pages can be stored on the host circuit monitor using ECC21

Product Line
ECC21
CM4000
CM3000

Environment
Webpage

Resolution
You can have up to 10 .html pages on the ECC21, if the firmware on the ECC21 is version 4.5 and the firmware on the CM4000/3000 is version 12.720 or higher. Older firmware of CM4/3 or ECC21 will only allow 5 .html pages to be stored on the host circuit monitor.

For an example of how to add wepages see FA232892.

Schneider Electric Saudi Arabia