Issue
How to format the disk on chip of a CM3000 or CM4000 series meter
Product Line
CM3000
CM4000
Environment
Configuring Hardware
Cause
When formatting of the chip is required
Resolution
Caution: Remember that if this CM is host to an ECC21 that all web pages will be lost.
The procedure to format the DOC is as follows. Using a modbus read/write utility:
- Setup Command Result Pointers:
- Write 8020 to register 8017
- Write 8021 to register 8018
- Write 8022 to register 8019
- Write 9020 to register 8000 to open an editing session.
- Verify commands:
- Verify register 8017 reads 9020
- Verify register 8018 reads 0
- Write 7010 to register 8000 to format the DOC
- Verify commands:
- Verify register 8017 reads 7010
- Verify register 8018 reads 0
- Write 1 to register 8001 to save changes.
- Write 9021 to register 8000 to close the editing session.This will cause a meter reset and the DOC will be formatted after the meter is reset
Note: After formatting the DOC, all files must be reconfigured using ION Setup or PME.
Released for:Schneider Electric Saudi Arabia