Issue
How long is the Rx timeout settings on the ION73XX meters
Product Line
ION7300
Environment
Product Specifications
Resolution
Rx timeout setting is not available in the communication module of ION 7330. It is hard-coded in firmware to 2 seconds by default.