{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

WebReach/Diagrams won't display bitmap; displays red x instead

Issue:
In Vista, a background or icon is displayed correctly, however, in webreach/Diagrams only a red X is displayed.

Product:
ION Enterprise 6.0
StruxureWare Power Monitoring 7.0
Power Monitoring Expert 7.2/8

Cause:
The program cannot display a file in Webreach/Diagams if name contains special characters such as "&".

Resolution:
Change the name of the file to alphanumeric charaters only.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.