Search FAQs
Is there a command available to remotely pause the EGX300?
Issue
Can the EGX300 be paused/stopped, temporarily, from updating its webpages and monitoring?
Product Line
EGX300
Environment
Webserver
Cause
This may be desirable, for instance, when a PLC needs to access for a read request.
Resolution
There is no command to temporarily stop the EGX from monitoring. However, if you navigate away from the monitoring pages, it will stop the EGX page communications to the slaves.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: