{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Struxureware Power Monitoring 7.0.1 - RepGen - Clicking the Summary button causes error about unregistered RICHTX32.ocx

Issue:
A user receives the following error after clicking on the Summary button when attempting to reate a new report using Reporter (RepGen - the excel based reporting tool):

Run time error '339'
*ERROR* Error 339 (Component 'RICHTX32.OCX' or one of its dependencies not correctly registered: a file is missing or invalid)

Product Line:
Struxureware Power Monitoring 7.0
Struxureware Power Monitoring 7.0.1

Environment:
"Reporter" report generation

Cause:
'RICHTX32.ocx' is not registered

Resolution:
To correct this issue, manually register richtx32.ocx using regsvr32.exe. Be sure to run this command when logged into the machine as the Administrator (not just an account that is in the Administrators group). On machines running a 64-bit version of the operating system, be sure to use the 32 bit version of regsvr32.exe. It will be located in the C:\Windows\SysWOW64 directory. Here are the steps:

1- Start a command prompt (Right click on it and "Run as administrator")
2- Navigate to the C:\Windows\SysWOW64 directory, then run the following command:
regsvr32 richtx32.ocx

You will see a dialog indicating the ocx registered successfully as shown in picture below. Once this is done, RepGen will function normally.


The next release (Power Monitoring Expert version 7.2 and higher) does not run into this problem and the file is registerd during installer.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.