{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Configuring PowerLogic Scada Web Client When the Server Network is Isolated from the Company Network.

Issue
How to configure Powerlogic Scada web client when the server network is isolated from the company network

Product Line
Powerlogic Scada 7.x
Power Scada Expert  8.x

Environment
Web client configuration

Cause
Powerlogic Scada project is not configured to handle the isolated network.

Resolution
The configuration for the Powerlogic Scada Web Client setup will be identical to a single NIC card setup.
The second NIC card needs to be added to the project and add the second NIC card added to the IOServers, Alarm Server, Trend Server, and Report Server.
To access the Web Client from a company PC, enter the IP address for the company network NIC card/citect and the Web Client will display.

Note: Port Forwarding configuration is only needed in Powerlogic Scada 7.10 setup. All other versions require just doing a Web Deployment normally.

Schneider Electric Saudi Arabia

Explore more
Range:
AVEVA™ Plant SCADAPowerLogic SCADA 7.10EcoStruxure™ Power SCADA Operation 8.2
Explore more
Range:
AVEVA™ Plant SCADAPowerLogic SCADA 7.10EcoStruxure™ Power SCADA Operation 8.2
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.