{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Power Monitoring Expert 7.2.x or PME 8.x - Upgrade fails at 'Verify Database' - The ION_Network table was not upgraded successfully

Issue:
When upgrading to Power Monitoring Expert 7.2.x or PME 8.x, the installer fails on the 'Verify Database' step, with the following message:

"The ION_Network table was not upgraded successfully"

Product Line:
Power Monitoring Expert
StruxureWare Power Monitoring 7.0.x
StruxureWare Power Monitoring 8.x
ION Enterprise

Environment:
Product Installer

Cause:
This problem can occur if the ION_Network database comes from a system that has been upgraded many times, and the original system was a version of ION Enterprise prior to 5.0. In old versions of ION Enterprise, the logical file name of ION_Network was PegasysNOM_Data and PegasysNOM_Log.

Open SQL Server Management Studio, right click on the ION_Network database and select 'Properties' to see what the Logical Names are for the database.



Resolution:
*Warning: Irreparable database damage can occur. This procedure should only be performed by users familiar with SQL Server Management Studio. Databases should be backed up prior to performing this procedure.*


To correct this issue, rename the Logical Name to ION_Network_Data and ION_Network_Log:



Once this is done, re-run the PME Installer.

NOTE: In some situations the ION_Network database contains both the ION_Network_Data and the PegasysNOM_Data logical names. Please see FA280826 for information on how to remove the extra database files.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.