{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Setting Address of SY/NET Devices such as PowerLogic Network Interface Modules (PNIM) etc.

The number of a Sy/Net device address on a SY/NET network cannot exceed the network size specified on the Sylink card. i.e. if the network size is set to 31 a PNIM cannot be addressed with the number 40.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: