{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What I/O comes with the portable Circuit Monitor Series 2000 , when you order the I/O option?

The optional factory installed input/output module used for the portable circuit monitor is the PCMIOM-44. The PCMIOM-44 has two status inputs, one mechanical relay output, and one KYZ output.


Legacy KB System (APS) Data: RESL185155 V2.0, Originally authored by KBAdPM on 06/27/2007, Last Edited by MaTh on 10/16/2010
Related ranges: CM2000 series

Schneider Electric Saudi Arabia