{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to set the system type of an Enercept Meter

Product Line
Enercept Meter

Environment
Voltage Mode Setup

Resolution
The factory default for the meter is a system type 40, but the following options are valid:

20 = Single Phase, 2 Wire
21 = Single Phase, 3 Wire
30 = Three Phase Delta
40 = Three Phase Wye

Write one of these values to the Single Holding Register 36.

Reference the video in FA180037 for information on how to write to registers.

Schneider Electric Saudi Arabia