{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to connect 3-Wire Modbus to an ION Meter

The Shield and GND (ground) connections are internally connected in an ION meter using a diode bridge.
Wiring diagram

This is the best wiring solution for connecting a 3-Wire RS-485 device to an ION Meter (COM1 or COM2).

NOTE: The fourth wire (Shield) should still be present in the communication wire bundle, but left unconnected at the ION meter.

Schneider Electric Saudi Arabia

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.