{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Is it possible to configure a Form 9S 8600/8650 meter as a Form 35S?

Issue
Customer purchased a ION 8600/8650 with "Form Factor" of 9/29/36S Base and wants to wire as a Form 35S

Product Line
ION86xx

Environment
Installation and wiring

Cause
Customer purchased 9s meter for use in form 35S environment

Resolution
It is possible to configure a form 9S ION 8600/8650 meter as a form 35S, but a form 35S cannot be converted into a 9S since
the form 35S meter does not have a blade for I2 connection.

Following the diagrams below, the meters connection terminals can be rewired to match.

The 9S meter is normally configured as bellow to accept a 3 Element 4Wire-Wye system.
As you can see, the blade inputs are used to accept the I1/I2/I3 & V1/V2/V3/Vref inputs for the 9S. A 35S meter only uses I1/I3 & V1/V3/Vref to meter the Delta system.

Form 9 and 9SFrom 35 and 35S

The 9S can be modified easily to simulate the 35S measurement structure as below:
Wiring diagram

This can be done by modifying your 9S base meter wiring as the image below:
3 Element Form 9 and 9S

The meter's Volts mode configuration setting, found in the Basic Setup Parameters, needs to be changed to 35S 3-Wire instead of 9S 4-Wire.
The firmware is the same for all types of form factors hence, it is not required to change the firmware.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: