{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Webreach navigation problems in Internet Explorer

Goals and Symptoms

When browsing the diagram with Webreach, for some reasons parts of the diagram don't work. Sometimes the historical logs don't show up. The same diagram seen from Vista works fine.

Facts and Changes

Webreach, browser, navigation

Causes and Fixes

The cause for this issue is that the IIS (Internet Information Services) has difficulties accessing the hierarchy of the different diagrams. Hence it is possible that during the session, the browser is lost and some links appear to be missing, or some queries don't execute properly. To avoid this issue, there are two possible workarounds:

  • Refrain from using the "Back" button in Internet Explorer. Using the back button uses the content of the cache file on the client, and doesn't make a new query to the IIS. Use the "Back to network diagram" button instead.
  • Make sure all the Objects or Datalog Viewers in Vista are set as "Custom Link" or "Custom Query Server" instead of "Inherit from parent window". When browsing the diagrams, the "Inherit..." option can cause the IIS to get lost.





Last Revised: November 19, 2007
Applies To: ION Enterprise, Webreach
Public
All content © 1992-2007 Schneider Electric

Legacy KB System (APS) Data: RESL189301 V1.0, Originally authored by KBAdPM on 11/20/2007, Last Edited by KBAdPM on 11/20/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5, ION Enterprise V5.0

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.