{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum length of a 73xx RMD cable?

The RMD cable for the 73xx series has only been tested at the 6' length.
It is possible to extend it to further lengths, but keep in mind that the further it is extended the larger the energy drop between the meter and RMD is. The RMD is powered across the cable, and the cable is used as a direct access buss, not a transmission line so there are no RS-232/RS-485 style long run level converters, it is a direct logic connection so length is critical.




Last Revised: November 16, 2007
Applies To: ION 7300/7330/7350
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189302 V1.0, Originally authored by KBAdPM on 11/20/2007, Last Edited by KBAdPM on 11/20/2007
Related ranges: ION7300

Schneider Electric Saudi Arabia