{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the operating temperature specs of the 73xx for both Tropical and non-Tropical forms?

Operation temperature of a 73xx series meter is -20°C to +60°C (-4°F to +140°F) ambient air, and is the same for both the Tropical and non-Tropical boards. In addition, Storage Temperature is 0°C (-22°F) to +85°C (185°F) and Relative Humidity is 5% to 95% RH non-condensing.

Last Revised: November 22, 2007
Applies To: ION 7300 / 7330 / 7350
Public
All content © 1992-2007 Schneider Electric


Legacy KB System (APS) Data: RESL189587 V1.0, Originally authored by KBAdPM on 11/23/2007, Last Edited by KBAdPM on 11/23/2007
Related ranges: ION7300

Schneider Electric Saudi Arabia