{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to get data from a 3rd-Party Microsoft SQL Database into ION Enterprise's VIP?

It is sometimes desirerable to get data from a database that is not part of ION Data into ION Enterprise, so that the Arithmetic Module in the VIP can be used for calculations and reporting.


  • This is possible. Lets say, for example, the user wants to get data from a 3rd party database into VIP and then do some kind of arithmetic calculation on it.

    The easiest way to do this is:
    • Move the data from SQL to Excel
    • Use an Excel OPC Server and the ION OPC Client to bring it into the VIP

    NOTE: The ION OPC Client is considered 'custom', and requires an Application Engineer to configure. Please contact your Sales Representative for more information.


Last Revised: December 7, 2007
Applies To: ION Enterprise
Public
All content © 1992-2007 Schneider Electric

Legacy KB System (APS) Data: RESL190281 V1.0, Originally authored by KBAdPM on 12/07/2007, Last Edited by KBAdPM on 12/07/2007
Related ranges: ION Enterprise V5.6, ION Enterprise V5.5, ION Enterprise V5.0

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.