Search FAQs
Can the Reports in ION Setup be viewed in local meter time?
No, ION Setup only displays reports in local PC time.
The workaround for this is to (temporarily) switch the computer to the same time zone as the meter.
- Double-click the clock in the lower right of the PC's toolbar and choose the 'Time Zone' tab
- Adjust this to the meters time zone
Last Revised: December 13, 2007
Applies To: ION Setup
Public
All content © 1992-2007 Schneider Electric
Legacy KB System (APS) Data: RESL190358 V1.0, Originally authored by KBAdPM on 12/13/2007, Last Edited by KBAdPM on 12/13/2007
Related ranges: ION Setup 2.1
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: