ION 6200 series Power Meters do support THD functionality with Enhanced Package 2, however, due to limitations in available memory space, this feature is not available when the Volts Mode is set to Delta or Delta Direct. Hence, when the ION6200 meter is used in these Volts Modes, the meter will return '0' for THD values both on the front panel display and through communications with the device.
It is recommended to use the PM750 or PM800 series meters instead if it is desired to get the THD values used in Delta or Delta Direct configurations.
Date Created: April 2, 2009
Last Revised: April 28, 2009
Public
Original Author: KG
All content © 1992-2009 Schneider Electric
Legacy KB System (APS) Data: RESL198374 V1.0, Originally authored by MiNe on 04/29/2009, Last Edited by MiNe on 04/29/2009
Related ranges: ION6200
Released for:Schneider Electric Saudi Arabia