{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to add or order additional digital I/O modules for the ION7300, ION7330, or ION7350 meters?

Issue
Is it possible to add or order additional digital I/O modules for the ION7300, ION7330, or ION7350 meters?

Product Line
ION 7300
ION 7330
ION 7350

Environment
Digital Inputs
Product Availability

Cause
Extra digital I/O modules for ION 73XX series meters

Resolution
No, it is not possible to add additional digital I/O modules for the ION7300 series meters. Only what is provided by default is available at this time.

Schneider Electric Saudi Arabia