{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does ION Enterprise v5.6 or v6.0 offer device support for SEPAM series 20, 40 and 80 relays?

SEPAM device support is only available for ION Enterprise version v5.6 Service Pack 2 (Released 8/28/08) and above, but is not included in the ION Enterprise v5.6 SP2 and ION Enterprise v6.0 software by default. These are optional devices that must be downloaded from the Powerlogic website:
For United States customers:
http://www.powerlogic.com/downloaddetail.cfm/cs/1/csec/2/fk_cat_id/2/fk_subcat_id/16/fk_p_id/30/fk_dc_id/0/fk_dsc_id/0/sub_id/98

For all other customers:
http://global.powerlogic.com/support/ION_Enterprise/optional_device_drivers/

Consult the powerlogic website for updates to device drivers or additional support additions


These optional device drivers contain a subset of the full Modbus register list available for each device type.

  • Only real-time reads from the device will be supported.
  • As part of the optional device download and installation, standard ION Vista diagram displays and predefined software-based data logging will be provided.
  • Software-based alarming will be available through the VIP module of ION Enterprise, and will require manual configuration.

No onboard device data logs, onboard alarm logs, onboard waveform captures (if available on the device), or device control (i.e. resets) are supported by optional devices.


Date Created: November 17, 2009
Last Revised: November 23, 2009
Public
Original Author: JJ
All content © 1992-2009 Schneider Electric

Legacy KB System (APS) Data: RESL200569 V1.0, Originally authored by MiNe on 11/24/2009, Last Edited by MiNe on 11/24/2009
Related ranges: ION Enterprise V6.0, ION Enterprise V5.6, Sepam series 80, Sepam series 40, Sepam series 20

AEDL3

Schneider Electric Saudi Arabia