{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum current for the Digital Inputs on an ION7300 series?

Issue:
Needs to know the current rating for the Digital Inputs on the ION7300 Series

Product Line:
ION7300 Series

Environment:
Digital IO of the ION7300 Series

Resolution
The maximum current a single Digital Input channel will draw is 0.9 mA. This assumes a 0 ohm load from Common to S1. If the resistance between the terminals is more, the current draw will be less. If all 4 contacts are closed, each channel will at most have 0.9 mA, with the Common having at most 3.6 mA.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.