Goals and Symptoms
In the Diagnostic Module, there is a register for Battery Remaining. Following is the information copied from ION Reference.
With the new v355 firmware release the ION7550/7650 will have this register populated. The register always existed but was never populated with the information.
Causes and Fixes
Please note:
In order to replace the battery:Refer to PowerLogic ION7550/7650 Battery Replacement Instructions Document # 70052-0253-00.
After following the above document, the battery remaining register needs to be reset at this point.
- Via Telnet (firmware older than v355)
2. Login=7600 or 7500, Password:<front panel password>
3. Press 9<Enter> to get into the debug parser.
4. Type HN<Enter> to reset the battery counter
- Via Telnet (firmware v355 and above)
2. Login= 7650 or 7550, Password:<front panel password>
3. Press 9<Enter> to get into the debug parser.
4. Type BATCLEAR<Enter> to reset the battery remaining register.
- Via Hyperterminal (firmware v355 and above)
2. Connect to COMx using Hyper Terminal
3. Login= 7600 or 7500, Password:<front panel password>
4. Press 9<Enter> to get into the debug parser.
5. Type BATCLEAR<Enter> to reset the battery remaining register.
- Via Hyperterminal (firmware older than v355)
2. Connect to COMx using Hyper Terminal
3. Login= 7650 or 7550, Password:<front panel password>
4. Press 9<Enter> to get into the debug parser.
5. Type HN<Enter> to reset the battery remaining register
For firmware v355 and above
Use BATSETCAPACITY command to set the new capacity when using a battery not shipped from our factory.
BATSTAT .....................………...Display Battery Stats
BATCLEAR ................................Reset Battery Counters
BATSETCAPACITY <mAh> ........Set Battery Capacity (mAh)
Note: Default battery capacity is 1500mAh.
Use command to set the new capacity when using a battery not shipped from our factory.
For firmware prior to v355
HB .....................………...Display Battery Stats
HN ...................................Reset Battery Counters
BATSETCAPACITY <mAh> ........Set Battery Capacity (mAh)
Note: Default battery capacity is 1500mAh.
Warning:
A dead battery or the act of changing/removing a battery may cause the following symptoms:
1) possible incorrect time
- resolved by performing a timesynch after as described in the Battery Replacement Instructions
2) possible incorrect battery remaining statistics (because time is a factor)
- resolved by following the steps in this document - the BATCLEAR or HN command
3) possible corrupt interval data (600 error in the event log)
- resolved by saving and restoring integrator data using ION Setup. Essentially the values in the integrator are copied manually and entered again.
Released for: Schneider Electric Saudi Arabia
Need help?
Start here!
Find answers now. Search for a solution on your own, or connect with one of our experts.
Contact Support
Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Search FAQs
Search topic-related frequently asked questions to find answers you need.
Contact Sales
Start your sales enquiry online and an expert will connect with you.