{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ION8600 v332 'Use GPS Quality Flag' Setup Register Added

Goals and Symptoms

A new setup register has been added to the clock module on the 8600. This register is named Use GPS Quality Flag. It has two settings, Use Flag and Ignore Flag.


Previous versions of firmware which were setup to synchronize to a GPS time source would only do so if the GPS was locked to a satellite source. If the source became unlocked, the meter would stop accepting time synchs until the lock was reacquired.

Causes and Fixes

The new setup register allows the user to select the behavior they want.



Use Flag: The meter will only accept time synchs if the source quality flag reports locked.
Ignore Flag: The meter will accept time synchs regardless of the quality flag state.

Attachments

(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/4db3753f9a0a42d1c125769c00161059/fl_block_5/0.1A60?OpenElement&FieldElemFormat=gif)
Date Created: December 10, 2009
Last Revised: December 29, 2009
Public
Original Author: SN
All content © 1992-2009 Schneider Electric


Legacy KB System (APS) Data: RESL200831 V1.0, Originally authored by MiNe on 12/30/2009, Last Edited by MiNe on 12/30/2009
Related ranges: ION8600

Schneider Electric Saudi Arabia