{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

RoHS compliance Information for ION meters

Issue
RoHS compliance information for ION Meters.

Product Line
ION6200, 6300, 7300, 7550, 7650, 8600 & 8800

Environment
Schneider Electric ION Meters

Cause
Customers complying with REACh regulations and that have environmental concerns need to be able to find accurate information regarding meter compliance.

Resolution
This application provides information about the products marketed by Schneider Electric relating to the European REACh regulation (substances content) and RoHS directives (hazardous substances), their environmental profile (PEP) and their End of life instructions (EOLI) based on their date codes.


The ION6200, 6300, 7300, 7550, 7650, 8600 & 8800 are RoHS compliant.

You can also type in the meter family in the Schneider Check a Product database to find the status. It is updated monthly. (to check the product, you should simply type "6200" for "ION6200", "7650" for "ION 7650"...etc).  For more information, contact your local Schneider representative.

Green Premium - Overview


Schneider Electric Saudi Arabia

Explore more
Range:
PowerLogic PM8000 seriesPowerLogic ION7550 | ION7650PowerLogic ION8800
Explore more
Range:
PowerLogic PM8000 seriesPowerLogic ION7550 | ION7650PowerLogic ION8800
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.