{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Utility for configuring a Micrologic trip unit remotely

Issue
Need to configure a trip unit before connecting to a monitoring or control software

Product Line
Masterpact, Powerpact, Compact NS, Compact NSX, Micrologic

Environment
Applications requiring the remote setting of breaker configuration.

Cause
Add setting parameters for a breaker before adding it to a power monitoring software like ION Enterprise or Power Monitoring Expert.

Resolution
Users can use the RSU (Remote Setting Utility) to configure their Micrologic trips. Below are the link to respective program for each class general type, standard and NSX.

Trip Units
Micrologic 2.0
Micrologic 3.0
Micrologic 5.0
Micrologic 2.0A
Micrologic 3.0A
Micrologic 5.0A
Micrologic 6.0A
Micrologic 7.0A
Micrologic 2.0E
Micrologic 3.0E
Micrologic 5.0E
Micrologic 6.0E
Micrologic 5.0P
Micrologic 6.0P
Micrologic 7.0P
Micrologic 5.0H
Micrologic 6.0H
Micrologic 7.0H

Use Masterpact RSU

https://www.se.com/download/ww/en/details/598291406-RSU-Remote-Setting-Utility---Masterpact-NTNW/?showAsIframe=false&reference=Micrologic_RSU_Masterpact_rev_853_Setup

Trip Units
Micrologic 2.2
Micrologic 2.3
Micrologic 3.2
Micrologic 3.3
Micrologic 5.2A
Micrologic 6.2A
Micrologic 5.3A
Micrologic 6.3A
Micrologic 5.2E
Micrologic 6.2E
Micrologic 5.3E
Micrologic 6.3E

Use Mircologic NSX RSU

https://www.se.com/download/hk/en/details/2331423-RSU-Remote-Setting-Utility---Compact-NSX/?showAsIframe=false&reference=Micrologic_RSU_Compact-NSX_rev_11139_Setup


RSU setup

RSU setup 2

Note
  • When the IFE module is used, its configuration website can be used to configure.

Schneider Electric Saudi Arabia