{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
When the user tries to add a device in Management Console, they see the error "Exception of type Management Console.Common.ManagementConsoleExxception' was thrown"

Goals and Symptoms

Issue
After a user has replaced a Network database with a new Network Database from the System\etc folder and then tries to add a device in Management Console, they may see the below (screenshot) error message:
Note: The error message will appear when the user tries to click on OK to save the setting.

=============================
Exception
---------------
Exception of type 'ManagementConsole.Common.ManagementConsoleException' was thrown.
<OK>
=============================

Causes and Fixes

Cause

This message can be caused by:

A. The ionsng.dll file has become corrupt

B. The user did not enter the Product Key for their ION software


Resolution

A. Re-register the ionsng.dll by following the steps in RESL189281
B. Enter the product key using the License Manager under TOOLS in Management Console, as shown below.


Legacy KB System (APS) Data: RESL201141 V2.0, Originally authored by KBAdPM on 01/26/2010, Last Edited by MaTh on 01/04/2013
Related ranges: ION Enterprise V6.0

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.