Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Error generated when running the "ION_Diag" diagnostics tool

Issue
When running the ION_Diag diagnostics program, the following error is generated referring to MinDate and MaxDate properties and the program will not run.



ion_Diag

Run-time error '35773':
A date was specified that does not fail within the MinDate and MaxDate properties.

Product Line 
ION Enterprise 5.5, 5.6
ION Enterprise 6.0.x

Cause
The error is a result of the transition to the year 2011. The Visual Basic form defines a MaxDate property for the date range desired for the system log which was set to 12/31/2010.

Resolution
Download and extract the attached version of ION_Diag and transfer it to the ION server.
Run the new version of ION_Diag.exe.

Schneider Electric Saudi Arabia

Attachment(s)
ION_Diag.zip [55.57 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.