Issue
How to determine the Serial number, MAC address or firmware version for the EM4800 meter.
Product
E4800 and EM4800
Environment
Web Browser
Resolution
1) Connect to the meter's web page using http://[IP address]
2) Click on the 'Info" menu option
3) Click on the "Manufacture" link
MAC address and serial number are also printed on product labels
Released for:Schneider Electric Saudi Arabia