Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
StruxureWare Power Monitoring 7.0.1: Database Upgrade FAQ


Upgrading ION-Enterprise to StruxureWare Power Monitoring (SPM) 7.0.1 requires the ION databases to be upgraded. If upgrading from version prior to SPM 7.0, this is a long-running operation. The new databases also require additional hard drive space.

The attached FAQ provides more information regarding time required to complete an upgrade, storage requirements, and developer/system integrator questions.

Note that the numbers given in the attached document in regards to drive size requirements for upgrade and final upgraded database size are based on internal tests only. These numbers may be adjusted in response to results from field upgrades. It's always best to err on the side of caution and provide much more space than is currently recommended.

Schneider Electric Saudi Arabia

Attachment(s)
SPM701-DatabaseUpgrade.pdf [729.81 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.