Issue
Data values from paralleled CT's
Product Line
PM800
CM3000
CM4000
Environment
Hardware
Cause
Data signals on the same line
Resolution
These meters monitor the Parallel CTs as a single combined total rather than as separate connection points. The meter will provide a combined total for the energy accumulation rather than a total per set of CTs.
Released for:Schneider Electric Saudi Arabia