Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
Where can I download the latest version of ION Setup software?

Issue
Latest version of ION Setup software Installer is required.

Product Line
ION Setup 3.x.x

Environment
Software Installation Files

Resolution
The latest version can be downloaded using the link below:  
ION Setup Software

The ION Setup Software, User Guide, and Device Configuration Guide can also be obtained by visiting link below
(Note: The latest version of ION Setup software may not be up-to-date from the link below):
ION Setup Software and Documents

ION Setup is only supported on Windows Vista and newer.1

Note that for the best compatibility, we strongly recommend that users run ION Setup on windows versions that are officially supported by Microsoft.
Kindly refer to the Microsoft link below for end of support information:

https://support.microsoft.com/en-us/lifecycle/search

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: