{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
I/O Server Name Length May Affect Performance When an I/O Server is Shut Down in PowerLogic SCADA v7.20

When shutting down one or several (not all) I/O servers, performance may decrease according to the length of I/O server names. The affect on performance has not been quantified, but could be noticeable.
The cause of the drop in performance is a function which compares a string (in this case, I/O server name) character by character. An I/O server name of "IOServer1" will have 9 comparisons, while a name of "IO1" will have only 3. This difference could have a noticeable affect on performance while one or several I/O servers is being shut down. There is no performance impact while I/O servers are running, so alarms, real-time data, etc. are not affected.

The recommended action is to use I/O server names that are as short as possible.

Keywords: PLSCADA, PL SCADA, PowerSCADA, Power SCADA, StruxureWare PowerSCADA Expert, SPE 7.2, 7.20


Legacy KB System (APS) Data: RESL210003 V1.0, Originally authored by AnVa on 12/13/2012, Last Edited by AnVa on 12/13/2012
Related ranges: PowerSCADA Expert 7.2

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.