Search FAQs
How to view waveforms from a CM3000/CM4000 (CM3 and CM4) series meter?
Issue
Need to view waveforms from the CM3/CM4.
Product Line
CM3000, CM4000
Environment
ION Setup
Power Monitoring Expert
Cause
Cannot export data using ION Setup.
Resolution
Waveforms in these Powerlogic meters can viewed in Power Monitor Expert Vista diagrams or inside the Web Applications Alarms tab for Power Monitoring Expert 9.0 and newer.
Unfortunately, the ION Setup program cannot be used to view capture waveforms. ION setup can only view waveforms on devices that have the proper ION framework to enable this function.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: