{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is Windows 7 Ultimate supported for PME 8.x, PME 7.2.x, SPM 7.0.x, or ION Enterprise 6.0.x?
Product line
Power Monitoring Expert 8.x
Power Monitoring Expert 7.2.x
StruxureWare Power Monitoring 7.0.x
ION Enterprise 6.0.x

Environment
Operating System Compatibility

Cause
A user would like to know if Windows 7 Ultimate is a supported operating system for the PME 8.x, PME 7.2.x, SPM 7.0.x and ION Enterprise 6.0.x software platforms.

Resolution
Both the 32 and 64 bit versions of Windows 7 Ultimate are supported for PME 8.x, PME 7.2.x, SPM 7.0.x and ION Enterprise 6.0.x installations.

Schneider Electric Saudi Arabia