{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
May the Energy Meter Communications Board be added to the Energy Meter in the field?

Issue
Can the Energy Meter Communications Board be added to the Energy Meter in the field?

Product Line
Energy Meter
Energy Meter Communication Board

Environment
Communications
Field Retrofit

Resolution
Yes, the Energy Meter Communication Board (EMCB) may be installed in the Energy Meter in the field.
See chapter 3 of the Energy Meter Communication Board Instruction Bulletin attached below.

Schneider Electric Saudi Arabia

Attachment(s)
Energy_Meter_Communication_Board.pdf [913.79 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.