{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
NOTICE: Using Multiple Clients to Communicate to an Ethernet NIM STBNIP2212
Issue
The purpose of this Resolution is to inform users of the Advantys Ethernet NIM of certain precautions when using the 'Master Controller' option.

In applications where two or more clients write to the same island but not to the same output modules on that island, a situation could occur in the event of a loss of communications (cable break).


Product Line
Units affected are:
STBNIP2212 Ethernet NIM's configured for more than one client but where no two clients write to the same output module.



Resolution
Refer to the attached Resolution for further details.

Schneider Electric Saudi Arabia

Attachment(s)
Mulitple_clients_to_Ethernet_NIM-resolution_attachment.doc [1.34 MB]