{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
4300 ACM Device Type

Issue
When attempting to add a 4300 ACM device to the ION Enterprise/SPM/PME network using Management Console, the 4300 ACM does not show up in the drop-down list of possible device types.

Product Line
Ion Enterprise
StruxureWare Power Monitoring (SPM)
Power Monitoring Expert (PME)
4300 ACM

Environment
Management Console

Cause
The 4300 ACM is not on the 'official' list of supported device types in the ION_Network database.

Resolution
When adding a 4300 ACM, select the 3300 ACM device type.  Once added as a 3300 device type, it will communicate properly in all versions of ION Enterprise/SPM/PME.
The dropdown list can also be modified to include the 4300 by following the instructions in the article How to add 4300 Device Type to ION Enterprise/SPM/PME

Schneider Electric Saudi Arabia