{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to activate the Configuration Report in ION Setup for the ION7550RTU Meter.

Issue:
The reports section in ION Setup is not activated by default for the ION7550RTU and therefore the meter configuration report is also not activated.

Product Line:
ION7550RTU Meter

Environment:
ION Setup 3.0

Cause:
This feature is deactivated by default.

Resolution:
In order to unhide the feature, open the QuickIon.cfg file for the ION7550RTU from the …\Schneider Electric\ION Setup\Tables\PML7550RTU directory with Notepad or any text editor software.
Change line 8
From: AssistantCount=9
To: AssistantCount=11

Displays(Assistant10) and Reports (Assistant11) do exist in the code, but they are hidden. Therefore, to unhide the feature, change the 9 to 11 in the AssistantCount line.

Schneider Electric Saudi Arabia