Issue
1. If the meter is powered up with a dead battery or a disconnected/loose battery it will show a checkerboard pattern on the screen for several seconds.
2. All configurations applied to the meter such as PT/CT ratios, Integrator values and other framework changes will be lost.
Product Line
ION7330 ION7350
Environment
Meter Behavior
Cause
When the battery is dead or disengaged and it is power cycled, the meter performs a factory initialization. A factory initialization causes the meter to lose its configuration data and custom template changes.
Resolution:
This issue cannot be fixed in the field. If you experience this issue and are unable to utilize the workaround below, please contact Schneider Electric or distributor to initiate an RMA to return the meter to the factory for battery replacement while available.
Workaround
Ensure the meter is not power cycled. This can be accomplished via a backup power supply such as a UPS.
Note: This behavior does not apply to the 7300-meter types, but the resolution is the same.
*Please note: The batteries on the 7330/7350 meter are meant to last for at least 10 years. The battery life can be checked from the front panel under Name Plate info. Option. Unfortunately, the battery life percentage indicator is meaningless if the battery is already dead, and the meter has been power cycled.*
Released for: Schneider Electric Saudi Arabia
Issue
1. If the meter is powered up with a dead battery or a disconnected/loose battery it will show a checkerboard pattern on the screen for several seconds.
2. All configurations applied to the meter such as PT/CT ratios, Integrator values and other framework changes will be lost.
Product Line
ION7330 ION7350
Environment
Meter Behavior
Cause
When the battery is dead or disengaged and it is power cycled, the meter performs a factory initialization. A factory initialization causes the meter to lose its configuration data and custom template changes.
Resolution:
This issue cannot be fixed in the field. If you experience this issue and are unable to utilize the workaround below, please contact Schneider Electric or distributor to initiate an RMA to return the meter to the factory for battery replacement while available.
Workaround
Ensure the meter is not power cycled. This can be accomplished via a backup power supply such as a UPS.
Note: This behavior does not apply to the 7300-meter types, but the resolution is the same.
*Please note: The batteries on the 7330/7350 meter are meant to last for at least 10 years. The battery life can be checked from the front panel under Name Plate info. Option. Unfortunately, the battery life percentage indicator is meaningless if the battery is already dead, and the meter has been power cycled.*
Released for: Schneider Electric Saudi Arabia




Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.
50多年来,施耐德电气一直引领配电创新。我们不断重新定义配电,以帮助您充分利用全新的分散化、低碳化和数字化能源模式。
EcoStruxure配电是我们的最新发展- 数字化、开放式架构,使我们的合作伙伴和客户能够轻松利用配电领域的最新突破技术,将可靠性、安全性、效率、可持续性和互联互通性提升至新高度。
借助施耐德电气EcoStruxure配电,您可以在一个架构与平台上获得数字化、互联互通的产品、应用、分析与服务等解决方案。