Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION 7650/7550: Response time from detecting a disturbance/transient to triggering a digital output

Issue
What is the response time from detecting a disturbance/transient to triggering a digital output?

Product Line
ION 7650
ION 7550

Environment
Digital Outputs
Power Quality Detection

Cause
To determine the response time of a digital output from a power quality event

Resolution
ION7550/7650 can do high-speed digital out triggering since the digital out module will update every half-cycle (i.e. 0.01s for 50Hz). Thus, when the transient module fires AnyTrig, the digital out module will respond within 0.01 seconds.

However, the actual amount of time from a sag/swell/transient on the line, to the digital output triggering is not a half-cycle. The half-cycle time represents the transient/sag/swell ION modules update rate. The actual chain of events is as follows:
1. Transient occurs during a sampling window (1/2 cycle)
2. DSP processes transient (1/2 cycle)
3. DSP transfers data to main processor, and main processor fires ION modules (1/2 cycle)
4. Digital out changes state (1ms for solid state digital outs, 8 to 15 ms for mechanical relays)

At 50 Hz, the total time for the solid-state digital out to change state based on a transient at the start of the sampling window, is 1.5 cycles + 1ms = 31ms.
At 60 Hz, the total time for the solid-state digital out to change state based on a transient at the start of the sampling window, is 1.5 cycles + 1ms = 26ms.

The sag/swell and transient modules can both be used to trigger digital outputs in this case, as they are both high-speed modules.

You can use a Pulse Merge Module to trigger the digital out from both at once. It is also likely you will need to use a One Shot Timer to turn the digital output off again.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Start here!

    Find answers now. Search for a solution on your own, or connect with one of our experts.

  • Contact Support

    Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Search FAQs

    Search topic-related frequently asked questions to find answers you need.

  • Contact Sales

    Start your sales enquiry online and an expert will connect with you.

I'd like to receive news and commercial info from Schneider Electric and its affiliates via electronic communication means such as email, and I agree to the collection of information on the opening and clicks on these emails (using invisible pixels in the images), to measure performance of Schneider Electric's communications and to improve them. For more details, please read our Privacy Policy.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Find our Offices
  • Get a Quote
  • Where to buy
  • Careers
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Investors
  • EcoStruxure
  • Job Search
  • Blog
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.