{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Where is the ION Diagnostics Tool (ION_Diag.exe) located in ION Enterprise?

Issue:
User would like to run the ION_Diag.exe application is in ION Enterprise, but may be unsure where it is located

Product:
ION Enterprise

Environment:
Software Diagnostics

Cause:
User would like to use ION_Diag.exe retrieve basic diagnostics and system information. The tremendously valuable information retrieved is compressed into a .cab file

Resolution:
The ION diagnostics tools is in the following directory (Where C:\ needs to be replaced with the drive letter that the ION Application is installed):
C:\Program Files\Schneider Electric\ION Enterprise\system\bin

To find the Diagnostics Tool for PME 7.2.x and PME 8.x, click on the following article: Video: How do I generate a diagnostic file for PME?

Schneider Electric Saudi Arabia