{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
170ENT11001 Ethernet Communication Adapter IP Assignment With 802.3 Framing

Issue
The purpose of this resolution is to inform 170ENT11001 Ethernet Communication Adapter product users of an issue when assigning an IP address to a 170ENT11001 using Bootp 802.3 Framing.

A problem has existed with the 170ENT11001 in Exec. versions 1.04 and lower where the IP address could not be assigned via Bootp or DHCP when using 802.3 Framing.


Product Line
170ENT11001


Resolution
Assigning an IP via DHCP using 802.3 Framing will not be fixed.
Changes to the Operating System files would be required but they are no longer supported by the vendor.

Schneider Electric Saudi Arabia

Attachment(s)
ENT11001_Exec_Load_Procedure.ZIP.zip [3.18 KB]