{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Should address 199 be assigned to a CM2000 meter?

Issue
A CM2000 can be assigned an address from 1-199; however, should address 199 be used?

Product Line
CM2000 Series

Environment
Meter Addressing

Resolution
Address "199" should always be reserved. The circuit monitor will accept 199, but this is the address that the Circuit Monitor defaults to in a failure situation.

For steps on setting the CM2000's device address, please refer to FA218954.

Schneider Electric Saudi Arabia