Search FAQs
Square D Current Transformer (CT) Installation Information
Issue
Customer may need more information about how current transformers operate and how they are typically installed
Product Line
Current Transformers
Environment
Metering/Power Monitoring
Resolution
*Warning: Installation and maintenance of this device should only be performed by qualified, competent personnel that have appropriate training and experience with high voltage and current devices. Failure to follow the instructions / warnings in the Meter Installation Guide can result in permanent damage to the meter, severe injury or death.
See also Video: Installing Current Transformers - CT orientation with regard to either "H1" designation, Arrow, or White Dot
See attached file
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: