Issue:
Problems may arise trying to connect using an optical probe to PowerLogic and ION Meters
Product Line:
PowerLogic and ION meters
Environment:
Optical port communications
Cause:
The serial settings for the connection are configured incorrectly, most notably in the timing settings of the probe.
Resolution:
Software Settings Used to Communicate with Optical Probes
SummaryThe following compatibility table provides communications settings for use with Optical Probe models and various Power Measurement software.
Probe PEGASYS NTMeter ShopPEGASYS 9xION EnterpriseION SetupION ReaderComments MicroTel PMC-250 YesYesYesYesYesYesexternal power via mouse plug MicroTel PMC-500 NoYes1Yes1Yes1Yes1Yes1external power via mouse plug uDataNet PMC-250-300 YesYesYesYesYesYesexternal power via mouse plug uDataNet PMC-500-300 NoYes1Yes1Yes1Yes1Yes1external power via mouse plug, DTR switch selectable uDataNet PMC-500-301 Yes2Yes3Yes3Yes3Yes3Yes3external power via mouse plug GE SmartCoupler SC-1 NoYes1Yes1Yes1Yes1Yes1Battery pack uses standard 9V battery ABB Unicom III NoNoNoNoYes4Yes4Self Powered -
- 1 - Requires DTR to be forced off via software settings.
2 - Requires DTR switch on probe to be set to the open position.
3 - Requires either DTR to be forced off via software settings or DTR switch on probe to be set to the open position.
4 - Requires both DTR to be forced off and RTS to be forced on (or vice versa) via software settings.
- 1 - Requires DTR to be forced off via software settings.
-
Released for: Schneider Electric Saudi Arabia
Issue:
Problems may arise trying to connect using an optical probe to PowerLogic and ION Meters
Product Line:
PowerLogic and ION meters
Environment:
Optical port communications
Cause:
The serial settings for the connection are configured incorrectly, most notably in the timing settings of the probe.
Resolution:
Software Settings Used to Communicate with Optical Probes
SummaryThe following compatibility table provides communications settings for use with Optical Probe models and various Power Measurement software.
Probe PEGASYS NTMeter ShopPEGASYS 9xION EnterpriseION SetupION ReaderComments MicroTel PMC-250 YesYesYesYesYesYesexternal power via mouse plug MicroTel PMC-500 NoYes1Yes1Yes1Yes1Yes1external power via mouse plug uDataNet PMC-250-300 YesYesYesYesYesYesexternal power via mouse plug uDataNet PMC-500-300 NoYes1Yes1Yes1Yes1Yes1external power via mouse plug, DTR switch selectable uDataNet PMC-500-301 Yes2Yes3Yes3Yes3Yes3Yes3external power via mouse plug GE SmartCoupler SC-1 NoYes1Yes1Yes1Yes1Yes1Battery pack uses standard 9V battery ABB Unicom III NoNoNoNoYes4Yes4Self Powered -
- 1 - Requires DTR to be forced off via software settings.
2 - Requires DTR switch on probe to be set to the open position.
3 - Requires either DTR to be forced off via software settings or DTR switch on probe to be set to the open position.
4 - Requires both DTR to be forced off and RTS to be forced on (or vice versa) via software settings.
- 1 - Requires DTR to be forced off via software settings.
-
Released for: Schneider Electric Saudi Arabia




Need help?
Start here!
Find answers now. Search for a solution on your own, or connect with one of our experts.
Contact Support
Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Search FAQs
Search topic-related frequently asked questions to find answers you need.
Contact Sales
Start your sales enquiry online and an expert will connect with you.