What is the best type of 10Base-FL Fiber for 10Base-FL communications
Product Line
ION Devices
Environment
Fiber Optic Communications
Cause
Some devices such as older (pre 2008) models of the ION7650 have a fiber-optic communication hardware ordering option
Resolution
These are the best specifications for the the fiber to be on the 10Base-FL port
* Multi-Mode fiber
* Wavelength: 850 nm
* Connector Type: ST
* Cladding: 62.5/125 um
* Max Length: 2000m
Note: For 100Base-FX communications see What type of 100Base-FX Fiber is Required for devices with fiber optic communications?
Released for: Schneider Electric Saudi Arabia


Need help?
Start here!
Find answers now. Search for a solution on your own, or connect with one of our experts.
Contact Support
Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Search FAQs
Search topic-related frequently asked questions to find answers you need.
Contact Sales
Start your sales enquiry online and an expert will connect with you.