{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Diagram for wiring a Sepam ACE-959 4-Wire Modbus RS485 I/F Module as 2-Wire.

Issue

Diagram for wiring an ACE-959 4-Wire Modbus RS485 I/F Module as 2-Wire.

Product Line
ACE-959, Sepam

Environment
Sepam Communications

Cause
The ACE959 interface provides an electrical interface between Sepam™
and a 4-wire RS485 communication network. It is the main network cable
branching box for connecting a Sepam with a CCA612 cable

Resolution

See the diagram below for details on the connection from a 4-wire RS485 to 2-wire RS485 connection using the ACE-959


Attachments

The attachment is the PDF version of the diagram above.

Original article# 3688
All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL185609 V2.0
Related ranges: ACE 9XX, Cabling and connection accessories

Schneider Electric Saudi Arabia

Attachment(s)
Diagram_for_wiring_an_ACE-959_4-Wire_modbus_RS485_I-F_Module_as_2-Wire-.pdf [91.44 KB]