{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
ACE969 Multi-Protocol Communication Interface Installation Sheet, Instruction Bulletin (ANSI), 63230-216-235A1, May 2007

Issue

ACE969 Multi-Protocol Communication Interface Installation Sheet, Instruction Bulletin (ANSI), 63230-216-235A1, May 2007
The ACE969 multi-protocol communication interfaces function with Sepam Series 20, 40, or 80. They have two communication ports to connect a Sepam to two independent communication networks:
The S-LAN (Supervisory Local Area Network) port to connect Sepam to a supervision network using one of the three following protocols:
IEC 60870-5-103
DNP3
RTU Modbus
The communication protocol is selected when setting Sepam parameters.
The E-LAN (engineering local area network) port, reserved for Sepam remote parameter setting and operation using the SFT2841 software
There are two versions of the ACE969 interfaces. Each has different S-LAN ports:
ACE969TP (Twisted Pair) is for connecting to an S-LAN network using a two wire RS485 connection
ACE969FO (Fiber Optic) is for connecting to an S-LAN network using a fiber-optic connection (star or ring)
The E-LAN port is always a two-wire RS485 connection.

 

see attachment


 

Schneider Electric Saudi Arabia

Attachment(s)
63230-216-235A1_ACE969_Install_Sheet.pdf [1.08 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.