{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Quick start for configuring the TCSEGDB23F24FA M340 Modbus Plus Proxy Module.

Issue

Quick start for configuring the 'TCSEGDB23F24FA' M340 Modbus Plus Proxy Module

Product Line
'TCSEGDB23F24FA' M340 Modbus Plus Proxy Module

Environment
Windows 7

Resolution
The following steps can be used to configure the' TCSEGDB23F24FA' M340 Modbus Plus Proxy
Module

  • Set the Modbus Plus address for the bridge using the rotary switch that are located on the back
of the module.
  • Connect to the module using the default MAC derived ethernet address.
  • Enter the default username (USER) and password (USER) to access the configuration/setup
web pages.
  • Click on 'Setup'.
  • Click on 'IP Setup'.
  • Enter the IP address parameters.
  • Click on 'Apply'.
  • Click on 'Save To Flash'.
  • Click on 'IP address' under the section labeled 'M340 Interface'.
  • Enter the IP address parameters.
  • Click on 'Apply'.
  • Click on 'Save To Flash'.
  • Click on 'Register Offsets' under the 'M340 Interface' section.
  • Fill in the appropriate parameters.
  • Select 'Legacy Compatability 0x 4x by 1' if you are communicating to a Modicon PLC.
  • Click on 'Apply'.
  • Click on 'Save To Flash'.
  • If applicable, click on the appropriate sections to be filled in under the section named 'Modbus Plus Peer Cop'

Schneider Electric Saudi Arabia